AXIS#.PL.KIWAITFORSETTLE
Description
When AXIS#.PL.KIWAITFORSETTLE is 1, the position integrator is activated only when the axis has settled, as defined by the keyword AXISx.MOTIONSTAT.SETTLED.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-13-01-000 |
General Information
Type |
Read/Write |
Description | Activates the position integrator only when the axis has settled. |
Units |
N/A |
Range |
0 – 1 |
Default Value |
0 |
Data Type |
N/A |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.PL.KIWAITFORSETTLE |
500ch |
15h |
Unsigned8 |
- |
- |
Read/Write |
No |
AXIS2.PL.KIWAITFORSETTLE |
510ch |
15h |
Unsigned8 |
- |
- |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
5924 |
1 |
5924 (0x1724) |
AXIS1.PL.KIWAITFORSETTLE |
Unsigned8 |
Read/Write |
Yes |
71460 |
2 |
5924 (0x1724) |
AXIS2.PL.KIWAITFORSETTLE |
Unsigned8 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.PL.KIWAITFORSETTLE |
5924 |
Unsigned8 |
Read/Write |
- |